4.11 Configuration Protection

Once the device has been configured, writes to register bit fields by the station host controller are typically no longer necessary. However, should the host controller encounter a fault, it is possible that incorrect firmware execution may result in errant writes to PHY registers resulting in misconfiguration that could interfere with system-wide communication among other nodes on the bus. For this reason, the LAN8670/1/2 includes a feature to prevent writes to all registers once configuration by the host controller is complete.

The Write Enable (WREN) bit in the Configuration Protection Control (CFGPRTCTL) register enables and disables (blocks) writes to the device configuration registers. Following reset, the Write Enable bit is set indicating that configuration protection is inactive and writing to all register bit fields is enabled. Once the host controller has configured the device , it must unlock the CFGPRTCTL register as described below before it may write a ‘0’ to the Write Enable bit to activate configuration protection and disable writing to all configuration register bit fields preventing changes to the configuration. When configuration protection is active, the only registers that may be written and modified are the Clause 22 MMD Control (MMDCTRL) and MMD Address/Data (MMDAD) registers. These are used to indirectly access registers within the various memory mapped devices, including the Configuration Protection Control register.

By default, the Configuration Protection Control register is locked and the Write Enable bit cannot be modified. Changing the Write Enable bit requires the Configuration Protection Control register to be unlocked. Unlocking the Configuration Protection Control register requires writing two unique key values in sequence to the Configuration Protection Control register. The host controller must first write a value of 5341h to the Configuration Protection Control register. Once written, the Key #1 Accepted (KEY1) status bit will be set. The host controller must then write a value of 535Ah to the Configuration Protection Control register resulting in the Key #2 Accepted (KEY2) status bit being set. If any value other than 535Ah is written after the first key value has been accepted, the LOCKED state is re-entered, the Key #1 Accepted status bit will be cleared and the unlocking process must be restarted. Additionally, writing to any register other than the Configuration Protection Control will also result in the register being locked again with the Key #1 Accepted status bit cleared. It is allowed to read this register before writing the second key to assure that the first key has been accepted. When both key values have been written in the correct sequence and accepted as indicated by both the KEY1 Accepted and KEY2 Accepted status bits being set, the Configuration Protection Control register is unlocked and the host controller may then write and modify the Write Enable bit, enabling or disabling writes to all register bit fields. When the Configuration Protection Control register is unlocked, a write to any register will cause the Configuration Protection Control register to immediately become locked again, this includes a write to the CFGPRTCTL register. If another register was written to when the CFGPRTCTL register is unlocked, it will become locked again and the WREN bit will remain the same as before being unlocked. See Figure 4-7.

Figure 4-7. Configuration Protection Control Register Lock/Unlock State Diagram