3.3.5 HCI UART Initialization Command
The following table provides the command syntax for HCI UART initialization command.
| Command Syntax | MCHPRT HCI 6 | |||||
|---|---|---|---|---|---|---|
| Example | MCHPRT HCI 6 Print out the reply | |||||
The following figure shows the example of HCI UART initialization command.