3.2.2 Bluetooth DTM
The following table provides the command syntax for Bluetooth DTM mode initialization.
| Command Syntax | MCHPRT DTM init | |||||
|---|---|---|---|---|---|---|
| Example | MCHPRT DTM init | |||||
The following figure shows the example of DTM initialization.

The following table provides the command syntax for DTM mode exit.
| Command Syntax | MCHPRT 9 5 |
|---|---|
| Example | MCHPRT 9 5 |
The following figure shows the example of DTM mode exit.