10.10.1 ECC Double-bit Error Detected (DED)
A read from the Flash memory that results in a PFM ECC DED causes the Prefetch module to return a bus exception error to the initiator. If that initiator is the CPU, it recognizes the bus exception error, prevents the instruction from executing, or read data from loading and generates an exception using the bus exception error vector.
When an ECC DED error occurs, the PFMDED bit (CHESTAT[27]) is set. The exception handling code can, then, check this bit to determine whether the PFM ECC DED event is causing an exception or not. The exception handler clears this bit in software.
Note: CPU instructions or data prefetched from the PFM is always loaded into the Prefetch module, even if a DED error is generated. The Prefetch module line containing the DED data is tagged as valid until the line is replaced.