20.4.6 Resetting the DMT
The DMT can be reset in two ways: one way is after a system Reset, and another way is by writing an ordered sequence to the DMT PRE-CLEAR (DMTPRECLR) register and DMT CLEAR (DMTCLR) register in a specific two-step sequence.
- The STEP1[7:0] bits in the DMTPRECLR register must be written as ‘
01000000’ (0x40). This action sets the “Enable for Clearing” state, which enables the DMT to be cleared by step 2. - The STEP2[7:0] bits in the DMTCLR register must be written as ‘
00001000’ (0x08). This can only be done if preceded by step 1 and if the DMT is in the open window interval.
- DMTCNT counter
- DMTPRECLR register
- DMTCLR register
- DMTSTAT register
If any value other than 0x40 is written to the STEP1x bits, the BAD1 bit in the DMTSTAT register will be set, and it causes a DMT event to occur. Any value other than 0x08 written to the STEP2x bits will cause the BAD2 bit to be set in the DMTSTAT register. Also, if step 2 is not preceded by step 1 or step 2 is not carried out in the open window interval, it causes the BAD2 flag to be set. Immediately, a DMT event will occur. In both these cases, the DMTEVENT bit in the DMTSTAT register will be set. Refer to the flowchart illustrated in the following figure.