17.3.8 LPCLK Divider
The low-power clock divider module provides the clock source for low-power domain (VDDBUKUPCORE) modules. There are two sources of sleep clock sources, such as 32 KHz and 32.768 KHz clock. These clock sources are either from LPRC, SOSC or derived from POSC/FRC modules, such as RTCC, which requires 32.768 KHz in the RTC mode; whereas, the Bluetooth link controller requires a 32 KHz clock to maintain the Bluetooth clock in the Standby Sleep mode. Therefore, if the LPCLK source is 32 KHz, the RTC divider must be 31.25, which the user can select using CFGCON4.VBKP_DIVSEL. If the LPCLK source is 32.768 KHz, program CFGCON4.MLPCLK_MOD to divide it by 1.024. See Power Management Unit (PMU) for low power mode from Related Links.