18.3.1.4 Dream Mode
In the Dream mode (or Sleep Walking mode), the CPU is clock gated but peripherals can be turned on on-demand by events related to those peripherals. No code is executed.
When the DRMEN bit in the OSCCON register is set, it allows the DMA controller to switch between the Idle mode and the Standby Sleep mode. When the OSCCON.SLPEN bit is set and the OSCCON.DRMEN bit is set, the CRU monitors the DMAC to ensure all transfers are complete before going into the Standby Sleep mode.
If OSCCON.SLPEN = ‘1’, OSCCON.DRMEN = ‘1’ and peripheral clock requests are active, the CRU goes into the Idle mode until all peripheral clock requests are non-active; at which time the CRU goes into the Standby Sleep mode.
If OSCCON.SLPEN is not set, the DRMEN bit has no affect as the DMA clocks are still running in the Idle mode.
If the CRU recognizes a wake/interrupt event whose priority wakes the DMA but not the CPU, the CRU transitions to the Idle mode. Therefore, the DMA can perform the needed operations and, when the DMA is finished, the CRU go backs to the Standby Sleep mode. During this time, the CPU is still asleep.
If the wake event is such that the CPU must handle the event, the whole system exits the Standby Sleep mode and transitions back to the Run mode.