7.6 Command Table
User Commands that serve as a convenient method to utilize the API's in Standalone 15.4
PHY component and facilitates switch between different modes in application. This
commands implementation can be found in Figure 7-45. app_phy_cmd_processor.c
app_phy_cmd_processor.c
file
under app_p2p_phy/app_phy_cmd_processor/src/ folder. The aforementioned file is
highlighted in the following figure. Note: Argument values/input
values alongside the Commands must be given in integer(unsigned/signed) unless
exceptionally mentioned as "in hex" in command table below. Some of the range
mentioned in the following Command Table description is based on PHY layer Pan
Information Base (PIB) attributes. PIB attributes are database of managed objects
pertaining to the PHY Layer. Refer IEEE 802.15.4 - 2003/2006 spec for more details
on PIB attributes of PHY layer.
Command | Description | Syntax & Range | Reference/Example |
---|---|---|---|
phyInit | PHY Layer Initialization | - | phyInit |
phyReset | Resets the PHY state machine and sets the default PIB value if requested | phyReset,<set default PIB values-true/false> |
phyReset,true |
phyEdScan | Energy detection scan start | phyEdScan, <set scan duration ranging from 0 to 14>(unit - symbols) | phyEdScan,8 |
getAttribute | Get PHY PIB attribute: Attribute id can be referred from PHY PIB attribute table (common command to set any PHY PIB attribute) | getAttribute, <attribute id (hex)> | getAttribute, <attribute id(hex)> Note: For Attribute ID refer to IEEE 802.15.4 spec - PHY PIB attributes
table. |
setAttribute | Set PHY PIB attribute (common command to set any PHY PIB attribute) | setAttribute, <attr id (hex)> |
Note: For Attribute ID refer to IEEE 802.15.4 spec
- PHY PIB attributes table.
|
getChannel | Get the Current Channel. | -- | getChannel |
setChannel | Set the Current Channel | setchannel, <11 – 26> | setChannel, 11 |
getChannelPg | Set the Channel Page | -- | getChannelPg |
setChannelPg | Set the Channel Page | setChannelPg, <0/2/16/171> | setChannelPg,0 |
getPanId | Get the PAN ID( INTRAPAN - 16bits) | -- | getPanId |
setPanId | Set Network PAN ID | setPanId, <panid in hex 0x0000-0xffff - 16bits> | setPanId,0x0001 |
getDestAddr | Get the destination short address (16 bits) | -- | getDestAddr |
setDestAddr | Set the destination short address (16 bits) | setDestAddr,<0x0000-0xffff - 16bits> | setDestAddr,0x0001 |
getExtDestAddr | Get the destination short address (64 bits) | -- | getExtDestAddr |
setExtDestAddr | Set the destination Long address (64 bits) | setExtDestAddr,<0x0000000000000000-0x7fffffffffffffff - 64bits> | setExtDestAddr,0x123456 |
getSrcAddr | Get Short Address – 16 bits | -- | getSrcAddr |
setSrcAddr | Set Short Address – 16 bits | setSrcAddr,<0x0000-0xffff> | setSrcAddr,0x0002 |
getIeeeAddr | Get IEEE Address – 64 bits | -- | getIeeeAddr |
setIeeeAddr | Set IEEE Address – 64 bits | setIeeeAddr,<0x0000000000000000-0x7fffffffffffffff - 64bits> | setIeeeAddr,0x1234567 |
getCsmaMode | Get the CSMA mode | -- | getCsmaMode |
setCsmaMode | Set the CSMA mode | setCsmaMode,<0-3> | setCsmaMode,0 |
getTxPwr | Get the Tx Power in DBm | -- | getTxPwr |
setTxPwr | Set the Tx Power in DBm | setTxPwr,<-12 to 14>(unit - DBm) | setTxPwr,3 |
getIeeeAddr | Get 64-bit address | -- | getIeeeAddr |
getFrameRetry | MAC level frame retries | -- | getFrameRetry |
setFrameRetry | Set the MAC level Frame Retry to be retried in case of transmission failure. | setFrameRetry, <0 – 7> | setFrameRetry,1 |
rxEnable | Receiver Enable | rxEnable , <Set TRX states PHY_STATE_RX_ON/PHY_STATE_TRX_OFF: true/false> | rxEnable ,true |
trxSleep | Put the transceiver to sleep | trxSleep, <sleep mode - sleep mode 1/deep sleep - false/true> | trxSleep, 0 |
trxWakeup | Wakeup the transceiver | -- | trxWakeup |
CCA | Perform CCA over the channel given by the user | CCA, <phychannel: 11-26> | CCA,11 |
updateDeviceTable | Update the Device table with info like short address, ieee address and corresponding device index. | updateDeviceTable, <device index (0-total no. of devices), short
address(0x0000-0xffff (16 bits)), ieee address(64 bits)> Note: Total No. of Devices = 64 (default, MACRO
associated : NUM_OF_DEVICES) |
updateDeviceTable,1,0x1234,0x1234567 |
readDeviceTable | Read the Device table info based on table index. | readDeviceTable, < device index – 255 – if entire list of devices in device table need to be displayed/specific index of the device table> | readDeviceTable, 2 =>read the device info at index
2 readDeviceTable, 255 =>read the device info of all the devices. |
+++ | Enter data mode | +++, <Time period in microseconds> | +++,1000000 =>[1000000usec = 1sec] |
&&& | Exit Data Mode | -- | &&& |
periodTestMode | Enter Periodic Test Mode | periodTestMode, <Time period in microsecs> | periodTestMode,1000000 |
contTestMode | Start Continuous Test Mode | -- | contTestMode |
perTestMode | Start PER Test Mode | -- | perTestMode |
throughputTestMode | Start ThroughputTest Mode | -- | throughputTestMode |
stopTestMode | Stop All Active application Test Modes (periodTestMode, contTestMode, perTestMode, throughputTestMode) | -- | stopTestMode |
updatePERTestPacketsCnt | Update PER test Packets | updatePERTestPacketsCnt,<0-4294967295 packets> | updatePERTestPacketsCnt,100 |
promTestMode | Enable promiscuous RX mode | -- | promTestMode |
updateThroughputTime | Update Throughput Timer | updateThroughputTime,<0-4294967295us> | updateThroughputTime,1000000 |
getFrameType | Type of frame to be TX/RX | -- | getFrameType |
setFrameType | Type of frame to be TX/RX | setFrameType,<0-5> | setFrameType, 0 |
phyCntTx | Starts continuous transmission on current channel | phyCntTx,<txMode-0/1-CW_MODE/PRBS_MODE>,<userandomcontent -true/false> | phyCntTx,0,true |
stopPhyCntTx | Stops continuous transmission on current channel | -- | stopPhyCntTx |
ConfigRxRPCMode | Configures the reduced power consumption mode | ConfigRxRPCMode,<true - To Enable the rxRPC mode, false - To disable the rx RPC mode> | ConfigRxRPCMode,true |
configAutoAck | Configures TRX for auto acknowledging the reserved frame | configAutoAck,<enableAACK-true/false> | configAutoAck,true |
getRSSIBaseVal | get the base RSSI value for respective radios | -- | getRSSIBaseVal |
getTrxStatus | get the status of the transceiver | -- | getTrxStatus |
configRxSensitivity | Configures receiver sensitivity level. This is used to desensitize the receiver | configRxSensitivity,<pdtlevel:0-15> | configRxSensitivity,0 |
Note: Addressing Mode is set to 16 bit type as default config in
application. (Can be modified using the API
app_P2P_Phy_setAddressModes
)Note: For more details on Standalone IEEE 15.4 PHY component. refer
API guide