12.11.1 Changing the Connector Operating Mode
The connector on the controller operates in the following three modes:
- HBA Mode: Exposes physical drives to the operating system
- RAID Mode: Exposes only RAID volumes to the operating system
- Mixed Mode: Exposes RAID volumes and physical drives to the operating system
Note: Use this option to change the behavior of the connector on
Adaptec Smart Storage Controller.
By default, products with RAID support are configured to operate in Mixed Mode. Mode
options vary depending on the configuration of the logical and physical devices on the
connector. For example, the connector mode cannot be switched to HBA mode if the
connector is already configured with a RAID volume. A reboot is required for connector
mode changes to take effect.
Note: Changing from Mixed Mode or HBA
Mode to RAID Mode removes access to the physical drives from the operating
system.
To change the connector mode from the connector level:
- In the Enterprise View, select a connector.
- On the ribbon, in the Controller
group, click Set Properties.
The Set Properties window opens.
- From the Mode drop-down list, change the connector mode
to RAID, HBA or Mixed.
-
Click OK.
-
Reboot the server.