9.10 Managing the Controller Password
After initial setup, the Set maxCrypto Configuration dialog box displays an Additional Settings tab that hosts the controller-password lifecycle operations. The Additional Settings tab is disabled when logged in as the maxCrypto user, unless the controller is in the locked state.