11.2.5 Clock Switch and Sleep
If the NOSC/NDIV bits are written with new values and the device is put to Sleep before
the clock switch completes, the switch will not take place and the device will enter
Sleep mode.
When the device wakes up from Sleep and CSWHOLD is clear (CSWHOLD = 0), the clock
switch will complete and the device will wake with the new clock active, setting
CSWIF.
When the device wakes from Sleep and CSWHOLD is set (CSWHOLD = 1), the
device will wake up with the old clock active, and the new clock source will be
requested again.
If Doze mode is in effect, the clock switch occurs on the next clock cycle regardless of whether or not the CPU is active during that clock cycle.
0)Note:
- CSWIF is asserted coincident with NOSCR; interrupt is serviced at OSC#2 speed.
- The assertion of NOSCR may not be seen by the user as it is only set for the duration of the switch.
1)Note:
- CSWIF may be cleared before or after clearing CSWHOLD.
Note:
- CSWIF may be cleared before or after rewriting NOSC; CSWIF is not automatically cleared.