3.1.8 RNBD Transparent UART Application PIN Settings:
- PIC18F47Q10 MCC Configuration -
Transparent Serial Example

Set Device Selection to RNBD as shown in below image
Make sure Sample Example Toggle button was Enabled
Expand Reference Examples and Select Transparant UART application
Since PIC18F47Q10 has only Two Instance of EUSART's the second EUSART was loaded Automatically for CDC UART (If Device has more Number of Instances will be listed accordingly to select the respective EUSART's)
Note:
- Transparent UART Application uses two instance EUSART1 & EUSART2 for data transfer
- Make sure Interrupt Driven was enabled for both EUSART1 & EUSART2.
- Important: EUSART Rx1/Tx1
& Rx2/Tx2 Uncheck Analog, Slew Rate & Input Level Control
checkboxes as shown below.
Configuration for PIC Transparent UART was completed click here for code generation steps.