1 Harmony 3 Peripheral Library Application Examples for SAM9X60 Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
Name | Description |
---|---|
ADC Automatic Window Comparison | This example application shows how to sample an analog input in polled mode and send the converted data to console using automatic window comparison of converted values |
ADC Low Power | This example application shows the different low power sleep modes available with Fast Wake up either enabled or disabled |
ADC Polling | This example application shows how to sample an analog input in polled mode and send the converted data to console |
ADC User Sequence | This example application shows how to sample three analog inputs using the user sequencer in software trigger mode and send the converted data to the console |
CAN Blocking | This example application shows how to use the CAN module to transmit and receive CAN messages in polling mode |
CAN Interrupt | This example application shows how to use the CAN module to transmit and receive CAN messages in interrupt mode |
CAN Interrupt with Timestamp | This example application shows how to use the CAN module to transmit and receive CAN messages in interrupt mode |
Clock Configuration | This example application shows how to configure the clock system to run the device at maximum frequency. It also outputs a prescaled clock signal on a GPIO pin for measurement and verification |
DBGU Blocking | This example application demonstrates how to use the DBGU peripheral to transfer a block of data in a blocking manner |
DBGU Interrupt | This example application demonstrates how to use the DBGU peripheral to transfer a block of data in a non-blocking manner |
DBGU Ring Buffer | This example application shows how to use DBGU peripheral in ring buffer mode |
FLEXCOM SPI EEPROM Read Write | This example application shows how to use the FLEXCOM module in SPI mode |
FLEXCOM SPI Self Loopback DMA | This example application shows how to use the FLEXCOM SPI peripheral with DMA to transmit and receive a block of data |
FLEXCOM TWI (I2C) EEPROM | This example application shows how to use the FLEXCOM module in TWI mode |
FLEXCOM USART Blocking | This example application shows how to use the FLEXCOM module in USART mode |
FLEXCOM USART Interrupt | This example application shows how to use the FLEXCOM module in USART mode |
FLEXCOM USART Ring Buffer | This example application shows how to use the FLEXCOM peripheral in USART ring buffer mode |
Low Power Modes | This example application shows how to enter low power modes of SAM9X60 MPU |
OTPC Read Write (Emulation) | This example application shows how to use the OTPC Peripheral library to perform OTP operations |
PIO Interrupt | This example application shows how to generate GPIO interrupt on switch press and release, and indicate the switch status using the LED |
PIO Polling | This example application shows how to poll the switch input, and indicate the switch status using the LED |
PIT Period Change | This example application shows how PIT period can be changed during run time |
PIT Polling | This example application shows how to use PIT counter in polling mode |
PIT Start Stop | This example application shows how PIT can be started and stopped at run time |
PIT64B Periodic Interrupt | This application shows how to use PIT64B counter in interrupt mode |
PWM Channels | This example demonstrates how to use the PWM peripheral to generate PWM signals |
RSTC Interrupt | This example application shows how to use the RSTC peripheral to generate an interrupt instead of generating a reset, when the Reset switch is pressed on board |
RSTC Reset Cause | This example shows how to use the RSTC peripheral to indicate the cause of the device reset |
RTC Alarm Interrupt | This example application shows how to use the RTC to configure the time and generate the alarm |
RTT Alarm Interrupt | This example application shows how to use the RTT to generate alarm interrupt |
RTT Periodic Interrupt | This example application shows how to use the RTT to generate periodic interrupts |
TC Capture Mode | This example application shows how to use the TC module in capture mode to measure duty cycle and frequency of an external input |
TC Compare Mode | This example application shows how to use the TC module in compare mode to generate an active low, active high, and toggle output on compare match |
TC Timer Mode | This example application shows how to use the TC module in timer mode to generate periodic interrupt |
TRNG Random Number | This example application shows how to use the TRNG Peripheral library to generate and read a random number |
WDT Timeout | This example application shows how to generate a Watchdog timer reset by emulating a deadlock |
XDMAC Memory Transfer | This example application shows how to use the XDMAC peripheral to do a memory to memory transfer and illustrates the usage of burst size to reduce the transfer time |