3.4 Initializing the WILC Device
- Insert the WILC1000 SD card device into the SD Card slot.
- Copy the wilc-sdio.ko (driver/net/wireless/microchip/wilc1000) to the root file system using the USB mass storage drive using the following commands:
$ mount /dev/sda1 /mnt
$ cp /mnt/wilc-sdio.ko .
- Initialize the WILC device by inserting the
wilc-sdio.komodule using the following command:
$ insmod wilc-sdio.ko
After successful completion of the process, the wlan0 interface is up and running.