4.4.1 Change the Kernel Size in U-Boot
The size of the newly build kernel will be different from the kernel size set in the u-boot environment variable and without changing the kernel size, the booting process will look for kernel image in wrong location and will fail to fetch the kernel image.
Update the new kernel image size in the u-boot environment variable bootcmd. Refer the
following steps:
- Right click the Image Tree Blob (
.itb) file and select properties to see the size, refer the following image for details:Figure 4-1. SAMA5D3 Xplained Properties - Convert the bytes to Hexadecimal number.
For Example: Hexadecimal value: 423D10
- Interrupt the booting process at
u-boot and edit the bootcmd variable and change the kernel image size by using
the following command:
=> edit bootcmdUpdate the size mentioned in thebootcmdvariable with the previously converted size:edit: nand read 0x24000000 0x00180000 0x423D10; bootm 0x24000000#kernel_dt - Save the changes by using the
following command:
=> saveenvThe following is the reply displayed after executing=> saveenvcommand:Saving Environment to NAND Erasing NAND Erasing at 0x140000 -- 100% complete. Writing to NAND OK OK - Boot the board by using the following
command:
=> boot