5 Software Description
The demo application uses the following:
- A Flash application with EEPROM settings for the ATA8510 RF transceiver
- A SAMC21 application with EEPROM settings for the ATA5831 transceiver
The following are the development platforms and tools:
- The user can develop the Flash application for the ATAB8510B remote sensor using MPLAB X IDE along with ATATMEL-ICE.
- The user can develop SAMC21-XPRO board application using MPLAB X IDE.
For more details on the source code for all the applications, refer to the ATA8510
Evaluation Kit (ATA8510-EK1) (ATA8510-EK1 Tool Package.zip)
and download the latest software from the Software section.