4.2 Remote Sensor Board (ATAB8510B)

The ATA8510 RF transceiver is placed on a key fob board. The following figure illustrates the RF transceiver board. A CR2032 coin cell battery (not included) powers this RF transceiver, which is mounted on the bottom of the board. The user can use the SW1 and SW2 buttons on the ATAB8510 board for initiating data telegram transmission. The LED flashes during a temperature measurement before transmitting the RF data telegram.

The ISP connector helps the user to do the following:
  • Flash and EEPROM programming
  • Flash application debugging of the ATA8510 RF transceiver
For more details about the Flash application development, refer to the ATA8510 Evaluation Kit (ATA8510-EK1) (ATA8510-EK1 Tool Package.zip) and download the latest software from the Software section.
Figure 4-2. Remote Sensor Board (ATAB8510B)
Figure 4-3. Coin Cell Battery (CR2032)
The following figure illustrates the details about remote sensor current consumption:
  • Current consumption profile over time
  • Current consumption for the measurement period with and without LED
  • Indicates current consumption measured at a room temperature of 24°C
During the temperature measurement period of 40 ms, the LED is switched ON in parallel, increasing the current consumption. The RF telegram transmission takes about 11 ms at a power level of 6 dBm, resulting in current consumption of about 9.4 mA. In OFF mode, the temperature sensor is switched OFF, and the resulting current is indicated by the ATA8510 RF transceiver current consumption. This OFF mode current is highly dependent on ambient temperature. For more details, refer to the ATA8510/15 Industrial Data Sheet (DS70005505).
Figure 4-4. Remote Sensor Current Consumption at 24°C
The following table summarizes battery life for a CR2032 and CR2450 coin cell without using the LED during temperature measurement at 20°C. The assumption is that the battery voltage drops from the initial value of 3V to 2V by the end of battery service. The manufacturer defines the self-discharge with typically 1% per year at an ambient temperature of 20°C. The battery life for this application primarily depends on the measurement interval Ts, which defines the duration of the OFF mode, whereas measurement and Transmit mode have fixed durations.
Table 4-2. Battery Life at 20°C
Interval Ts (s)Mean Current (mA) Battery Lifetime (Days/Years)
CR2032 (230 mAh)CR2450 (560 mAh)
DaysYearsDaysYears
20.0531800.54371.2
50.0224451.210833.0
100.0118752.421315.8
200.00616964.6413011.3
500.002388010.6944825.9