3.3 Signal Timing
The following figure illustrates the signal timing of the data transfer.
- The remote sensor transmits a data telegram with duration of 11 ms every 10s or when the user presses the SW1 or the SW2 button (TX1). The preamble duration is 7 ms while the data payload duration is 4 ms. Then, the remote sensor switches into Receive mode with a time-out period of 20 ms (RX).
- The base station is polling for a valid RF signal that matches the RF channel, the data rate, the modulation scheme and the correct data encoding every 5 ms. This polling interval is chosen to match with the length of the preamble. When the base station receives a valid telegram (RX1), it acknowledges this telegram (TX) and waits for an acknowledgment frame from the remote sensor with the Remote Sensor signal strength data and a time-out of 90 ms (RX2).
- The remote sensor transmits the acknowledgment frame with the RSSI signal strength (TX2), then switches into OFF mode.
- If the base station does not receive
any acknowledgment packet from the remote sensor within 400 ms timeout, the base
station displays the error message, as shown below, on ATOLED1-XPRO OLED and changes
its mode from RX mode to Polling mode to poll for the temperature telegram.
RF telegram error: NoRF ACK telegram! - The base station reads the acknowledgment frame with the RSSI data (RX2), displays the result, then switches back into the Polling mode.