4.1 Hardware Setup
This example uses the following development boards:
- An AVR EA Curiosity Nano (EV66E56A)
- A Curiosity Nano Adapter Board (AC164162)
- An Ammonia Click™ by MikroElektronika (MIKROE-4151)
- A Buzz 2 Click by MikroElektronika (MIKROE-2720)
- A 2x2 Click by MikroElektronika (MIKROE-2152)
With the power off, insert the clicks as follows:
- Slot 1: Ammonia Click
- Slot 2: Buzzer Click
- Slot 3: 2x2 Click
Then, insert the AVR EA Curiosity Nano into the Curiosity Nano adapter, with the USB port facing outwards, as shown in the figure below.
Before use, it is important to turn the sensitivity of the Ammonia Click down as low as possible, as the sensor output may exceed the absolute maximum input voltage in extreme conditions. But more realistically, the click output could exceed the Analog to Digital Converter's (ADC) input range and cause the system to operate incorrectly.