An on-chip temperature sensor is available. To do a temperature
measurement, follow these steps:
Configure the voltage
reference to internal 1.024V by writing to the Reference Selection
(REFSEL) bit field the ADCn.CTRLC register.
Select the temperature
sensor as input in the Positive Input Multiplexer (ADCn.MUXPOS)
register.
Configure the ADC Sample
Duration by writing a value ≥ to the Sample Duration (SAMPDUR) bit
field in the Control E (ADCn.CTRLE) register.
Acquire the temperature
sensor output voltage by running a 12-bit Single-Ended
conversion.
Process the measurement
result, as described below.
The measured voltage has a linear relationship to the temperature. Due to
process variations, the temperature sensor output voltage varies between the
individual devices at the same temperature. The individual compensation factors
determined during the production test are stored in the Signature Row:
SIGROW.TEMPSENSE0 is a
gain/slope correction
SIGROW.TEMPSENSE1 is an
offset correction
The result of the temperature sensor measurement must be processed in the
application software using compensation values from device production or user
calibration to achieve more accurate results. Refer to the Electrical
Characteristics section for further details.
The following equation gives the temperature (in Kelvin):
It is recommended to follow these steps in the user code when
using the compensation values from the Signature
Row:
int8_t sigrow_offset = SIGROW.TEMPSENSE1; // Read signed offset from signature row
uint8_t sigrow_gain = SIGROW.TEMPSENSE0; // Read unsigned gain/slope from signature row
uint16_t adc_reading = ADC0.RESULT >> 2; // 10-bit MSb of ADC result with 1.024V internal reference
uint32_t temp = adc_reading - sigrow_offset;
temp *= sigrow_gain; // Result might overflow 16-bit variable (10-bit + 8-bit)
temp += 0x80; // Add 256/2 to get correct integer rounding on division below
temp >>= 8; // Divide result by 256 to get processed temperature in Kelvin
uint16_t temperature_in_K = temp;
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.