1.13 EEPROM Read Write
This example application demonstrates how to use the EEPROM peripheral library.
Description
This example uses the EEPROM peripheral library to perform the following operations:
- Performs write of 512 bytes of data into EEPROM and verifies the values by reading back
 - Performs page erase and verifies by reading
 - Performs bulk erase and verifies by reading
 
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/eeprom/eeprom_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32mk_gp_db.X | MPLABX project for PIC32MK GP Development Kit | 
| pic32mk_mcm_curiosity_pro.X | MPLABX project for PIC32MK MCM Curiosity Pro Board | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32mk_gp_db.X | PIC32MK GP Development Kit | 
| pic32mk_mcm_curiosity_pro.X | PIC32MK MCM Curiosity Pro Board | 
Setting Up PIC32MK GP Development Kit
- Connect the Debug USB port (J12) on the board to the computer using a micro USB cable
 
Setting Up PIC32MK MCM Curiosity Pro Board
- Connect the Debug USB port (J500) on the board to the computer using a micro USB cable
 
Running the Application
- Build and program the application project using its IDE
 - The LED is turned ON when the EEPROM Write, Read, Erase and Bulk Erase is
                        completedFollowing table provides LED names:
Board LED Name PIC32MK GP Development Kit LED1 PIC32MK MCM Curiosity Pro Board LED1