15.4.2 HSM Parameter Configuration

To use Job Manager in the HSM flow, U-HSM parameters must be set. These parameters are stored in the user-level DEF file and automatically loaded for any new or existing Job Manager project.

U-HSM configuration data specifies:

  • IP address of the U-HSM server
  • U-HSM UUID assigned by Microchip
  • U-HSM Master Key UUID
  • Default location of the keyset repository (see the Libero SoC Design Flow User Guide )
  • M-HSM UUID assigned by Microchip

The set_hsm_params Tcl command is used to configure HSM. See Tcl Interface for details.