21.5.5 hdl_core_delete_parameters
(Ask a Question)Description
This Tcl command deletes parameters from a HDL core definition. After this command usage It will be impossible to configure parameters of HDL core.
The command will fail if the module name or parameter list are not specified or are incorrect.
hdl_core_delete_parameters -hdl_core_name { module_name } \
-parameters { parameter_list }
Arguments
Parameter | Type | Description |
---|---|---|
hdl_core_name | string | Specify the HDL core name from which you want to delete parameters. This is a mandatory argument. |
parameters | list of strings | Specify the list of parameters from a HDL core. This is typically done to remove parameters from the list of parameters that was automatically extracted using the "hdl_core_extract_ports_and_params" command. This is a mandatory argument. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'hdl_core_name' is missing. |
None | Required parameter 'parameters' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'hdl_core_delete_parameters -hdl_core_name "hdl core name" -parameters "[parameter list]+"' |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
The following example deletes "WIDTH" parameters from a "test_hdl_core" HDL core definition:
hdl_core_delete_parameters -hdl_core_name {test_hdl_core} \
-parameters {WIDTH}
See Also
hdl_core_extract_ports_and_parameter