21.5.2 remove_hdl_core

Description

This Tcl command removes and HDL core component from the current project. The command will fail if the module name is not specified or is incorrect.

remove_hdl_core -hdl_core_name { hdl_core_name }

Arguments

ParameterTypeDescription

hdl_core_name

string

Specify the module name from which you want to delete a core component. This is a mandatory argument.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Required parameter 'hdl_core_name' is missing.

None

Parameter 'param_name' is not defined. Valid command formatting is ' remove_hdl_core -hdl_core_name "hdl core name"'.

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4

Example

The following example removes 'test_hdl_core' HDL core component:

remove_hdl_core -hdl_core_name {test_hdl_core}