21.4.23 sd_delete_nets

Description

This tcl command deletes one or more nets from the SmartDesign component.

Important: This command will not delete multiple nets in this release. Support for deleting multiple nets will be provided in the next Libero release. This command is not required to build a SmartDesign component. This command maps to an interactive user action in the SmartDesign Canvas and will not be present in the exported SmartDesign component Tcl description.
sd_delete_nets -sd_name {smartdesign component name} \
               -net_names {net names}

Arguments

ParameterTypeDescription

sd_name

string

Specifies the name of the SmartDesign component. It is mandatory.

net_names

string

Specifies the net names to be deleted. It is mandatory.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Required parameter 'sd_name' is missing.

None

The component 'design_name' doesn't exist.

None

Net 'net_name' does not exist.

None

Parameter 'net_names' has illegal value.

None

Required parameter 'net_names' is missing.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4™
SmartFusion® 2
IGLOO® 2

Example

This example deletes "B_REN_0" net from "top" design.

sd_delete_nets -sd_name {top} -net_names {B_REN_0}

See Also

  • sd_create_scalar_net
  • sd_create_bif_net