21.4.55 sd_update_instance

Description

This Tcl command updates an instance in a SmartDesign with its latest definition. This command is useful when the interface (port-list) of the component/module instantiated in a SmartDesign has changed. This command can be used to update any type of instance such as instances of other SmartDesign components, core components, HDL modules and HDL+ cores in a SmartDesign.

Note:

This command is not required to build a SmartDesign component. It maps to an interactive user action in the SmartDesign Canvas and will not be present in the 'Export Component Description(Tcl)' but will present in Libero Project 'Export Script File'.

sd_update_instance -sd_name {smartdesign component name} \
                   -instance_name {instance name}

Arguments

ParameterTypeDescription

sd_name

string

Specifies the name of the SmartDesign component. It is mandatory.

instance_name

string

Specifies the name of the instance to be updated. It is mandatory.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Required parameter 'sd_name' is missing.

None

Required parameter 'instance_name' is missing.

None

The component 'comp_name' doesn't exist.

None

Parameter 'param_name' is not defined. Valid command formatting is 'sd_update_instance -sd_name "sd_name" -instance_name "instance_name"'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4™
SmartFusion® 2
IGLOO® 2

Example

This example updates 'dff' instance in a 'top' SmartDesign with its latest definition:

sd_update_instance -sd_name {top} -instance_name {dff}

See Also

  • sd_instantiate_component