21.4.47 sd_set_inst_synth_attr

Description

This Tcl command sets synthesis attribute to the specified instance of the specified SmartDesign. The attribute is added in the HDL file at the component generation.

sd_set_inst_synth_attr \
        -sd_name {SmartDesign component name} \
        -instance_name {instance name} \
        -attr_name {synthesis attribute name} \
        -attr_value {synthesis attribute value}

Arguments

ParameterTypeDescription
sd_namestringThis argument is used to specify the name of the SmartDesign component in which the port synthesis attribute is set. This is a mandatory argument.
instance_namestringName of the instance in SmartDesign that synthesis attribute is added to. This is a mandatory argument.
attr_namestringSynthesis attribute. This is a mandatory argument.
attr_valuestringValue of the attribute. Some attributes do not require values.

Synthesis Attributes

The following is the list of attributes and directives available in the Synopsys® FPGA synthesis tool that are supported by SmartDesign.

Name Object Attribute/Directive
syn_insert_buffer port, instance Attribute
syn_keep net Directive
syn_maxfan port, net, instance, register Attribute
syn_no_compile_point module/architecture Attribute
syn_noclockbuf port, net, module/architecture Attribute
syn_noprune instance, module/architecture Directive
syn_preserve register, port, module/architecture Directive
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneInstance 'instance_name' does not exist.
NoneParameter 'instance_name' has illegal value.
NoneRequired parameter 'instance_name' is missing.
NoneParameter 'attr_value' has illegal value.
NoneRequired parameter 'attr_value' is missing.
NoneParameter 'attr_name' has illegal value.
NoneRequired parameter 'attr_name' is missing.
NoneParameter 'sd_name' has illegal value.
NoneRequired parameter 'sd_name' is missing.
NoneParameter 'param_name' is not defined. Valid command formatting is 'sd_set_inst_synth_attr -sd_name "sd_name" -attr_name "attr_name" -attr_value "attr_value" -instance_name "instance_name"'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4™
SmartFusion® 2
IGLOO® 2

Example

This example sets "syn_insert_buffer" attribute with "none" value on the "COREABC_C0_0" instance in the "top" design.

sd_set_inst_synth_attr -sd_name {top} -attr_name {syn_insert_buffer} \
                       -attr_value {none} -instance_name {COREABC_C0_0}

See Also

  • sd_remove_inst_synth_attr