21.4.54 sd_show_bif_pins

Description

This tcl command exposes one or more internal scalar or bus pins/ports of a Bus Interface pin/port. A Bus Interfacepin/port is usually a group of normal scalar or bus pins/ports grouped together and used to connect instances thathave similar interfaces.

Note:

This command will not expose multiple pins/ports in release v2021.1. Support to expose multiple scalar or bus pins/portswill be provided in the next Libero release.

sd_show_bif_pins -sd_name {smartdesign component name} \
                 -bif_pin_name {name of the bif pin or port} \
                 -pin_names {pins or ports to be exposed}

Arguments

ParameterTypeDescription

sd_name

string

Specifies the name of the SmartDesign component. It is mandatory.

bif_pin_name

string

Specifies the name of the Bus Interface pin/port for which the internal pins/ports need to be exposed. It is mandatory.

pin_names

string

Specifies the names of the Bus Interface internal pins/ports to be exposed. It is mandatory.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Parameter 'pin_names' has illegal value.

None

Required parameter 'pin_names' is missing.

None

Parameter 'bif_pin_name' has illegal value.

None

Required parameter 'bif_pin_name' is missing.

None

Parameter 'sd_name' has illegal value.

None

Required parameter 'sd_name' is missing.

None

Parameter 'param_name' is not defined. Valid command formatting is 'sd_show_bif_pins -sd_name "sd_name" -bif_pin_name "bif_pin_name" -pin_names "pin_names"'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4™
SmartFusion® 2
IGLOO® 2

Example

This example exposes "COREAXI4INTERCONNECT_C0_0:MASTER0_AWADDR" pin for "COREAXI4INTERCONNECT_C0_0:AXI4mmaster0" bif pin.

sd_show_bif_pins -sd_name {top} \
                 -bif_pin_name {COREAXI4INTERCONNECT_C0_0:AXI4mmaster0} \
                 -pin_names {COREAXI4INTERCONNECT_C0_0:MASTER0_AWADDR}

See Also

  • sd_delete_bif_pin