21.4.12 sd_create_bif_net

Description

This tcl command creates a bus interface (BIF) net in a SmartDesign component. Any net created must be connected to two or more ports/pins using the command “sd_connect_net_to_pins”.

Note: This command is not required to build a SmartDesign component. It is not exported when you select Libero Project - `Export Script File’ or ‘Export Component Description(Tcl)’ on a SmartDesign component. This command is used to manually create a Tcl script and specify a new name to the net that connects two or more ports/pins.
sd_create_bif_net -sd_name {smartdesign component name} \
                  -net_name {net name}

Arguments

ParameterTypeDescription
sd_namestringSpecifies the name of the SmartDesign component. It is mandatory.
net_namestringSpecifies the name of the net to be added in the SmartDesign component. It is mandatory. The command will fail if there is an already existing net with the same name.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneParameter 'net_name' has illegal value.
NoneRequired parameter 'net_name' is missing.
NoneParameter 'sd_name' has illegal value.
NoneRequired parameter 'sd_name' is missing.

None

Cannot add net "bus_net" because a net with the same name already exists.

None

Cannot connect the two bus interface pins 'BIF_1' and 'instance:BIF_1' because they are not compatible.
NoneParameter 'param_name' is not defined. Valid command formatting is 'sd_create_bif_net -sd_name "sd_name" -net_name "net_name"'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4™
SmartFusion® 2
IGLOO® 2

Example

This command creates BIF net named "bifnet1" in the "TOP" SmartDesign component.

sd_create_bif_net -sd_name {TOP} -net_name {bifnet1}

See Also

  • sd_connect_net_to_pins