21.8.4 check_constraints

Description

Checks all timing constraints in the current scenario for validity. This command performs the same checks as when the constraint is entered through SDC or Tcl.

When a constraint file is checked, the Constraint Checker does the following:
  • Checks the syntax.
  • Compares the design objects (pins, cells, nets, ports) in the constraint file versus the design objects in the netlist (RTL or post-layout ADL netlist). Any discrepancy (for example, constraints on a design object which does not exist in the netlist) are flagged as errors and reported in the *_sdc.log file.
check_constraints

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4™

Example

The following example checks timing constraints in the current scenario.

check_constraints