21.8.52 set_clock_latency

Description

Defines the delay between an external clock source and the definition pin of a clock within SmartTime.

Clock source latency defines the delay between an external clock source and the definition pin of a clock within SmartTime. You can specify both an "early" delay and a "late" delay for this latency, providing an uncertainty which SmartTime propagates through its calculations. Rising and falling edges of the same clock can have different latencies. If only one value is provided for the clock source latency, it is taken as the exact latency value, for both rising and falling edges.

Clock latency is of two types:
  • External latency (source) - From an external source to on-chip clock definition point using the -source argument.
  • Internal latency (network) - From a clock generator to an end point (FF) due to clock tree synthesis (CTS).

In FPGA, internal clock latency is not used because the clock tree is already inserted and Libero SoC tool is already aware of the delay. Hence, set_clock_latency is primarily used to model external latency in FPGA.

When external clock latency is modeled using the -source arguments, hold calculations are never impacted because the hold checks occur for the same clock edge. Setup times are only impacted when the -early and -late arguments are used because otherwise the clock is uniformly delayed to all endpoints in the design. The following table summarizes the behavior:
-source used-early used-late usedResult
YesNoNoNo setup or hold impact
YesNoYesNo setup or hold impact
YesYesNoNo setup or hold impact
YesYesYesSetup check only
NoN/AN/ANot recommended for FPGA designs.
Setup time is calculated for a scenario where the launch edge is delayed and the capture edge is early:
  • The -early value is added from the required time.
  • The -late value is added to the arrival time
set_clock_latency -source [-rise] [-fall] [-early] [-late] delay clock

Arguments

ParameterTypeDescription
sourceNoneSpecifies the source latency on a clock pin, potentially only on certain edges of the clock.
riseNoneSpecifies the edge for which this constraint will apply. If neither or both rise and fall are passed, the same latency is applied to both edges.
fallNoneSpecifies the edge for which this constraint will apply. If neither or both fall and rise are passed, the same latency is applied to both edges.
lateNoneOptional. Specifies that the latency is late bound on the latency. The appropriate bound provide the most pessimistic timing scenario. However, if the value of -late is less than the value of -early, optimistic timing takes place which could result in incorrect analysis. If neither or both -early and -late are provided, the same latency is used for both bounds, which results in the latency having no effect for single clock domain setup and hold checks.
earlyNoneOptional. Specifies that the latency is early bound on the latency. The appropriate bound provide the most pessimistic timing scenario. However, if the value of -late is less than the value of -early, optimistic timing takes place which could result in incorrect analysis. If neither or both -early and -late are provided, the same latency is used for both bounds, which results in the latency having no effect for single clock domain setup and hold checks.
delayfloating pointSpecifies the latency value for the constraint.
clockstringSpecifies the clock to which the constraint is applied. This clock must be constrained.

Error Codes

Error CodeDescription
Error: SDC0061Invalid clock latency constraint: Parameter has illegal value invoked from within command.

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4™

Example

The following example sets an early clock source latency of 0.4 on the rising edge of main_clock. It also sets a clock source latency of 1.2, for both the early and late values of the falling edge of main_clock. The late value for the clock source latency for the falling edge of main_clock remains undefined.

set_clock_latency –source –rise –early 0.4 { main_clock }
set_clock_latency –source –fall 1.2 { main_clock }

Related Examples on GitHub

See Also