21.8.60 set_input_delay

Description

Creates an input delay on a port list by defining the arrival time of an input relative to a clock in the current scenario.

The set_input_delay command sets input path delays on input ports relative to a clock edge. This usually represents a combinational path delay from the clock pin of a register external to the current design. For in/out (bidirectional) ports, you can specify the path delays for both input and output modes. The tool adds input delay to path delay for paths starting at primary inputs.

A clock is a singleton that represents the name of a defined clock constraint. This can be:

  • a single port name used as source for a clock constraint.
  • a single pin name used as source for a clock constraint; for instance reg1:CLK. This name can be hierarchical (for instance, toplevel/block1/reg2:CLK).
  • an object accessor that will refer to one clock: [get_clocks {clk}].
Note:
  • The behavior of the -add_delay option is identical to that of PrimeTime(TM).
  • If, using the -add_delay mechanism, multiple constraints are otherwise identical, except they specify different -max or -min values
    • The surviving -max constraint will be the maximum of the -max values.
    • The surviving -min constraint will be the minimum of the -min values.
set_input_delay delay_value -clock clock_ref [–max] [–min] [–clock_fall] [-rise] [-fall] [-add_delay] \
input_list

Arguments

ParameterTypeDescription
delay_valuerealSpecifies the arrival time in nanoseconds that represents the amount of time for which the signal is available at the specified input after a clock edge.
clockstringSpecifies the clock reference to which the specified input delay is related. This is a mandatory argument.
maxNoneSpecifies that the delay_value refers to the longest path arriving at the specified input. If you do not specify -max or -min options, the tool assumes maximum and minimum input delays to be equal.
minNoneSpecifies that the delay_value refers to the shortest path arriving at the specified input. If you do not specify -max or -min options, the tool assumes maximum and minimum input delays to be equal.
clock_fallNoneSpecifies that the delay is relative to the falling edge of the clock reference. The default is the rising edge.
riseNoneSpecifies that the delay is relative to a rising transition on the specified port(s). If -rise or -fall is not specified, then rising and falling delays are assumed to be equal.
fallNoneSpecifies that the delay is relative to a falling transition on the specified port(s). If -rise or -fall is not specified, then rising and falling delays are assumed to be equal.
add_delayNoneSpecifies that this input delay constraint should be added to an existing constraint on the same port(s). The -add_delay option capture information on multiple paths with different clocks or clock edges leading to the same input port(s).
input_listlist of stringProvides a list of input ports in the current design to which delay_value is assigned. If you need to specify more than one object, enclose the objects in braces ({}).
Return TypeDescription
integerReturns the ID of the clock input delay constraint.

Error Codes

Error CodeDescription
Error: SDC0004clk does not match any clock name or source.
Error: SDC0015port list [get_ports {CLK_0_D}] is incorrect.
Error: SDC0054Invalid IO delay constraint: the min delay is greater than max delay.
Error: SDC0061Parameter _AtclParam0_ has illegal value.

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4™

Example

The following example sets an input delay of 1.2 ns for port data1 relative to the rising edge of CLK1.

set_input_delay 1.2 -clock [get_clocks CLK1] [get_ports data1]

The following example sets a different maximum and minimum input delay for port IN1 relative to the falling edge of CLK2.

set_input_delay 1.0 -clock_fall -clock CLK2 –min {IN1}
set_input_delay 1.4 -clock_fall -clock CLK2 –max {IN1}

The following example demonstrates an override condition of two constraints. The first constraint is overridden because the second constraint specifies a different clock for the same input.

set_input_delay 1.0 -clock CLK1 –max {IN1}
set_input_delay 1.4 -clock CLK2 –max {IN1}

The next example is almost the same as the previous one, however, in this case, the user has specified -add_delay, so both constraints will be honored.

set_input_delay 1.0 -clock CLK1 –max {IN1}
set_input_delay 1.4 -add_delay -clock CLK2 –max {IN1}

The following example is more complex:

  • All constraints are for an input to port PAD1 relative to a rising edge clock CLK2. Each combination of {-rise, -fall} x {-max, -min} generates an independent constraint. But the max rise delay of 5 and the max rise delay of 7 interfere with each other.
  • For a -max option, the maximum value overrides all lower values. Thus the first constraint will be overridden and the max rise delay of 7 will survive.
set_input_delay 5 -max -rise -add_delay [get_clocks CLK2] [get_ports PAD1] # will be overridden
set_input_delay 3 -min -fall -add_delay [get_clocks CLK2] [get_ports PAD1]
set_input_delay 3 -max -fall -add_delay [get_clocks CLK2] [get_ports PAD1]
set_input_delay 7 -max -rise -add_delay [get_clocks CLK2] [get_ports PAD1]

Related Examples on GitHub

See Also