21.8.59 set_false_path

Description

Identifies paths that are considered false and excluded from the timing analysis in the current timing scenario. The set_false_path command identifies specific timing paths as being false. The false timing paths are paths that do not propagate logic level changes. This constraint removes timing requirements on these false paths so that they are not considered during the timing analysis. The path starting points are the clocks, the input ports or register clock pins, and the path ending points are the clocks, the register data pins or output ports. This constraint disables setup and hold checking for the specified paths.

The false path information always takes precedence over multiple cycle path information and overrides maximum delay constraints. If more than one object is specified within one -through option, the path can pass through any objects.

You must specify at least one of the –from, -to, or –through arguments for this constraint to be valid.

set_false_path [-ignore_errors] [-from from_list ] [-through through_list ] [-to to_list ]

Arguments

ParameterTypeDescription
ignore_errorsNoneSpecifies to avoid reporting errors for derived constraints targeting the logic that becomes invalid due to logic optimization. It is an optional argument. Some IPs may have extra logic present depending on other IPs used in the design but the synthesis tool will remove this logic if fewer IPs were used. In such cases, the implementation flow will halt without -ignore_errors flag.
Note: It is not recommended to use this flag outside similar use cases.
fromlist of stringsSpecifies a list of timing paths starting points. A valid timing starting point is a clock, a primary input, an inout port, or a clock pin of a sequential cell.
throughlist of stringsSpecifies a list of pins, ports, nets, or instances (cells) through which the disabled paths must pass.
tolist of stringsSpecifies a list of timing paths ending points. A valid timing ending point is a clock, a primary output, an inout port, or a data pin of a sequential cell.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
Error: SDC0021Invalid false path constraint: the -from value is incorrect.
Error: SDC0022Invalid false path constraint: the -from is empty.
Error: SDC0024Invalid false path constraint: the -to is empty.
Error: SDC0026Invalid false path constraint: the -through is empty.
Warning:cell (get_cells) is incorrect type; -through objects must be of type net (get_nets), or pin (get_pins).
Note: Constraint will be disabled.
Warning:port (get_ports) is incorrect type; -through objects must be of type net (get_nets), or pin (get_pins).
Note: Constraint will be disabled.

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4™

Example

The following example specifies all paths from clk1 clock to data pins of a specific register reg_2 as false paths.

set_false_path –from [get_clocks {clk1}] –to reg_2:D

The following example specifies all paths through the pin U0/U1:Y to be false.

set_false_path -through U0/U1:Y

The following example specifies a derived false path constraint through the PCIe_Demo_0/SYSRESET_POR/POWER_ON_RESET_N pin.

set_false_path -ignore_errors -through [ get_pins {PCIe_Demo_0/SYSRESET_POR/POWER_ON_RESET_N } ]

Related Examples on GitHub

See Also