21.8.42 remove_max_delay

Description

Removes a maximum delay constraint from the current timing scenario by specifying either its exact arguments or its ID. If the arguments do not match a maximum delay constraint in the current scenario, or if the specified ID does not refer to a maximum delay constraint, this command fails.

Do not specify both maximum delay arguments and the constraint ID.

remove_max_delay [-from from_list] [-to to_list] [-through through_list]
remove_max_delay -id constraint_ID

Arguments

ParameterTypeDescription
fromlist of stringsSpecifies a list of timing path starting points. A valid timing starting point is a clock, a primary input, an inout port, or a clock pin of a sequential cell.
throughlist of stringsSpecifies a list of pins, ports, cells, or nets through which the disabled paths must pass.
tolist of stringsSpecifies a list of timing path ending points. A valid timing ending point is a clock, a primary output, an inout port, or a data pin of a sequential cell.
idintegerSpecifies the ID of the maximum delay constraint to remove from the current scenario. You must specify either the exact maximum delay arguments to remove or the constraint ID that refers to the maximum delay constraint to remove.

Error Codes

Error CodeDescription
NoneInvalid arguments -from/-to/-through.
NoneOnly one argument is needed.

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4™

Exceptions

You cannot use wildcards when specifying a clock or port name, either alone or in an accessor command.

Example

The following example specifies a range of maximum delay constraints to remove.

remove_max_delay -through U0/U1:Y

Related Examples on GitHub

See Also