21.8.24 list_input_delays

Description

Returns details about all of the input delay constraints in the current timing constraint scenario.

list_input_delays

Arguments

Return TypeDescription
stringDetails about all of the input delay constraints in the current timing constraint scenario.

Supported Families

PolarFire®
PolarFire SoC
SmartFusion® 2
IGLOO® 2
RTG4™

Example

With this command we get the details about all of the input delay constraints in the current timing constraint scenario.

puts [list_input_delays]

Related Examples on GitHub

See Also