TCPIP_UDP_DestinationPortSet Function

C

bool TCPIP_UDP_DestinationPortSet(UDP_SOCKET s, UDP_PORT remotePort); 

Returns

  • true - Indicates success
  • false - Indicates an invalid socket

Description

This function sets the destination port, which allows changing the destination port dynamically.

Remarks

The destination remote port will always be changed, even if remotePort == 0. It will not change the UDP_OPTION_STRICT_PORT on the socket.

Preconditions

UDP initialized UDP socket should have been opened with TCPIP_UDP_ServerOpen/TCPIP_UDP_ClientOpen. hUDP - valid socket

Parameters

ParametersDescription
hUDPthe UDP socket
remotePortdestination port to use