TCPIP_UDP_TxOffsetSet Function

C

bool TCPIP_UDP_TxOffsetSet(UDP_SOCKET hUDP, uint16_t wOffset, bool relative); 

Returns

  • true - if the offset was valid and the write pointer has been moved
  • false - if the offset was not valid

Description

This function allows the write location within the TX buffer to be specified. Future calls to TCPIP_UDP_Put, TCPIP_UDP_ArrayPut, TCPIP_UDP_StringPut, etc will write data from the indicated location.

Preconditions

UDP socket should have been opened with TCPIP_UDP_ServerOpen/TCPIP_UDP_ClientOpen. hUDP - valid socket

Parameters

ParametersDescription
hUDPUDP socket handle
wOffsetOffset in the UDP packet data payload to move the write pointer.
relativeif true, the wOffset is added to the current write pointer. else the wOffset is from the beginning of the UDP buffer