TCPIP_UDP_SocketInfoGet Function
C
bool TCPIP_UDP_SocketInfoGet(UDP_SOCKET hUDP, UDP_SOCKET_INFO* pInfo);
Returns
- true - if the call succeeded
- false - if no such socket or invalid pInfo
Description
This function will fill a user passed UDP_SOCKET_INFO structure with current status of the selected socket.
Preconditions
UDP socket should have been opened with TCPIP_UDP_ServerOpen()/TCPIP_UDP_ClientOpen()(). hUDP - valid socket pInfo -valid address of a UDP_SOCKET_INFO structure
Parameters
Parameters | Description |
---|---|
UDP_SOCKET | hUDP Socket for which information is to be obtained |
UDP_SOCKET_INFO* | pInfo pointer to UDP_SOCKET_INFO to receive socket information |