TCPIP_UDP_SocketNetSet Function
C
bool TCPIP_UDP_SocketNetSet(UDP_SOCKET hUDP, TCPIP_NET_HANDLE hNet);
Returns
- true - Indicates success
- false - Indicates failure
Description
This function sets the network interface for an UDP socket
Remarks
A NULL hNet can be passed (0) so that the current socket network interface selection will be cleared If the hNet != 0, it will enforce UDP_OPTION_STRICT_NET on the socket.
Preconditions
UDP socket should have been opened with TCPIP_UDP_ServerOpen/TCPIP_UDP_ClientOpen. hUDP - valid socket
Parameters
Parameters | Description |
---|---|
hUDP | The UDP socket |
hNet | interface handle |