DRV_ENC28J60_Process Function

C

TCPIP_MAC_RES DRV_ENC28J60_Process(DRV_HANDLE hMac); 

Returns

  • TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid
  • TCPIP_MAC_RES_OP_ERR - if the hMac is valid

Description

ENC28J60 Process This function does additional processing that is not done inside the tasks function.

Remarks

This function does nothing in the first release.

Preconditions

The client had to be successfully opened with DRV_ENC28J60_Open.

Parameters

ParametersDescription
hMacthe successfully opened handle