DRV_ENC28J60_RxFilterHashTableEntrySet Function
C
TCPIP_MAC_RES DRV_ENC28J60_RxFilterHashTableEntrySet(DRV_HANDLE hMac, const TCPIP_MAC_ADDR* DestMACAddr);
Returns
- TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid
- TCPIP_MAC_RES_OP_ERR - if the hMac is valid
Description
ENC28J60 Receive Filter Hash Table Entry Set This function adds to the MAC's hash table for hash table matching.
Remarks
This functionality is not implemented in the first release.
Preconditions
The client had to be successfully opened with DRV_ENC28J60_Open.
Parameters
Parameters | Description |
---|---|
hMac | the successfully opened handle |
DestMACAddr | MAC address to add to the hash table |