DRV_ENC28J60_Status Function

C

SYS_STATUS DRV_ENC28J60_Status(SYS_MODULE_OBJ obect); 

Returns

  • SYS_STATUS_ERROR - if an invalid handle has been passed in
  • SYS_STATUS_UNINITIALIZED - if the driver has not completed initialization
  • SYS_STATUS_BUSY - if the driver is closing and moving to the closed state
  • SYS_STATUS_READY - if the driver is ready for client commands

Description

ENC28J60 Status This function will get the status of the driver instance.

Preconditions

The driver had to be successfully initialized with DRV_ENC28J60_Initialize().

Parameters

ParametersDescription
objectThe object valid passed back to DRV_ENC28J60_Initialize()