DRV_ENC28J60_StatisticsGet Function
C
TCPIP_MAC_RES DRV_ENC28J60_StatisticsGet(DRV_HANDLE hMac, TCPIP_MAC_RX_STATISTICS* pRxStatistics, TCPIP_MAC_TX_STATISTICS* pTxStatistics);
Returns
- TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid
- TCPIP_MAC_RES_OP_ERR - if the hMac is valid
Description
ENC28J60 Get Statistics Get the current statistics stored in the driver.
Remarks
Statistics are not planned for the first release.
Preconditions
The client had to be successfully opened with DRV_ENC28J60_Open.
Parameters
Parameters | Description |
---|---|
hMac | the successfully opened handle |