1.2.5.2.53 TCPIP_MAC_StatisticsGet Function

C

TCPIP_MAC_RES TCPIP_MAC_StatisticsGet(
    DRV_HANDLE hMac, 
    TCPIP_MAC_RX_STATISTICS* pRxStatistics, 
    TCPIP_MAC_TX_STATISTICS* pTxStatistics
);

Description

This function will get the current value of the statistic counters maintained by the MAC driver.

Precondtions

TCPIP_MAC_Initialize() should have been called. TCPIP_MAC_Open() should have been called to obtain a valid handle.

Parameters

ParametersDescription
hMacHandle identifying the MAC driver client.
pRxStatisticsPointer to a TCPIP_MAC_RX_STATISTICS that will receive the current RX statistics counters. Can be NULL if not needed.
pTxStatisticsPointer to a TCPIP_MAC_TX_STATISTICS that will receive the current TX statistics counters. Can be NULL if not needed.

Returns

  • TCPIP_MAC_RES_OK - If all processing went on OK.
  • TCPIP_MAC_RES_OP_ERR error code - If function not supported by the driver.

Remarks

The reported values are info only and change dynamically.