1.2.5.2.35 TCPIP_MAC_ParametersGet Function
C
TCPIP_MAC_RES TCPIP_MAC_ParametersGet(
DRV_HANDLE hMac,
TCPIP_MAC_PARAMETERS* pMacParams
);
Description
This is a function that returns the run time parameters of the MAC driver.
Precondtions
TCPIP_MAC_Initialize() should have been called. TCPIP_MAC_Open() should have been called to obtain a valid handle.
Parameters
Parameters | Description |
---|---|
hMac | Handle identifying the MAC driver client. |
pMacParams | Address to store the MAC parameters. |
Returns
- TCPIP_MAC_RES_OK - If pMacParams updated properly.
- TCPIP_MAC_RES_OP_ERR error code - If processing failed for some reason.
Remarks
None.