DRV_MIIM_Tasks Function
C
void DRV_MIIM_Tasks(SYS_MODULE_OBJ object); Returns
None
Description
This function is used to maintain the driver's internal state machine.
Remarks
This function is normally not called directly by an application. It is called by the system's Tasks routine (SYS_Tasks)
This function will never block or access any resources that may cause it to block.
Preconditions
The DRV_MIIM_Initialize routine must have been called for the specified MIIM driver instance.
Example
SYS_MODULE_OBJ object; // Returned from DRV_MIIM_Initialize
while (true)
{ DRV_MIIM_Tasks (object);
// Do other tasks
}