DRV_MIIM_ClientStatus Function
C
DRV_MIIM_CLIENT_STATUS DRV_MIIM_ClientStatus(DRV_HANDLE handle); Returns
DRV_MIIM_CLIENT_STATUS_READY - if the client handle represents a valid MIIM client
DRV_MIIM_CLIENT_STATUS_ERROR - if the client handle is an invalid MIIM client
Description
This function gets the client-specific status of the MIIM driver associated with the given handle.
Remarks
This function can be used to check that a client handle points to a valid MIIM client. The MIIM driver queues operations so it will always return DRV_MIIM_CLIENT_STATUS_READY.
Preconditions
The DRV_MIIM_Initialize routine must have been called.
DRV_MIIM_Open must have been called to obtain a valid opened device handle.