TCPIP_SMTP_StringPut Function
C
uint16_t TCPIP_SMTP_StringPut(
char* Data
);
Description
This function writes a string to the SMTP client.
Preconditions
TCPIP_SMTP_UsageBegin() returned true on a previous call.
Parameters
| Parameters | Description |
|---|---|
| Data | The data to be written. |
Returns
The number of bytes written. If less than the length of Data, then the TX FIFO became full before all bytes could be written.
Remarks
This function should only be called externally when the SMTP client is generating an on-the-fly message. (That is, TCPIP_SMTP_MailSend() was called with SMTPClient.Body set to NULL.)