TCPIP_DHCPV6_SERVER_STATUS_CODE Enumeration
C
typedef enum {
TCPIP_DHCPV6_SERVER_STAT_SUCCESS = 0,
TCPIP_DHCPV6_SERVER_STAT_UNSPEC_FAIL = 1,
TCPIP_DHCPV6_SERVER_STAT_NO_ADDRS_AVAIL = 2,
TCPIP_DHCPV6_SERVER_STAT_NO_BINDING = 3,
TCPIP_DHCPV6_SERVER_STAT_NOT_ON_LINK = 4,
TCPIP_DHCPV6_SERVER_STAT_USE_MULTICAST = 5,
TCPIP_DHCPV6_SERVER_STAT_MAX_CODE = 5,
TCPIP_DHCPV6_SERVER_STAT_EXT_ERROR = -1
} TCPIP_DHCPV6_SERVER_STATUS_CODE;
Description
DHCPv6 server status code.
Members
| Members | Description |
|---|---|
| TCPIP_DHCPV6_SERVER_STAT_SUCCESS = 0 | Success. |
| TCPIP_DHCPV6_SERVER_STAT_UNSPEC_FAIL = 1 | Failure, reason unspecified; this status code is sent by either a client or a server to indicate a failure not explicitly specified in the RFC. |
| TCPIP_DHCPV6_SERVER_STAT_NO_ADDRS_AVAIL = 2 | Server has no addresses available to assign to the IA(s). |
| TCPIP_DHCPV6_SERVER_STAT_NO_BINDING = 3 | Client record (binding) unavailable. |
| TCPIP_DHCPV6_SERVER_STAT_NOT_ON_LINK = 4 | The prefix for the address is not appropriate for the link to which the client is attached. |
| TCPIP_DHCPV6_SERVER_STAT_USE_MULTICAST = 5 | Sent by a server to a client to force the client to send messages to the server using the All_DHCP_Relay_Agents_and_Servers address. |
| TCPIP_DHCPV6_SERVER_STAT_MAX_CODE = 5 | Maximum valid value. |
| TCPIP_DHCPV6_SERVER_STAT_EXT_ERROR = -1 | An error occurred, status code not found, etc. |