TCPIP_TFTPS_EVENT_HANDLER Type
C
typedef void (* TCPIP_TFTPS_EVENT_HANDLER)(TCPIP_NET_HANDLE hNet, TCPIP_TFTPS_EVENT_TYPE evType, const char* name, const void* param);
Description
Type: TCPIP_TFTPS_EVENT_HANDLER The format of a notification handler registered with the TFTP server module. Once an TFTP server event occurs the TFTP server service will be called for the registered handler.
Remarks
If pNetIf == 0, the notification is called for events on any interface.
Parameters
Parameters | Description |
---|---|
hNet | the interface on which the DNS event occurred |
evType | the TFTP server reported event |
name | the host name associated with the event |
param | additional user parameter - see TCPIP_TFTPS_HandlerRegister |